Start
> notebooks/laptops
> Acer LX.AHG0X.041
|
 |
Aspire 5720 G-102G16Mi |
|
Brand: Acer
Product code: LX.AHG0X.041
EAN/UPC code: 0099802078645
|
Category: notebooks/laptops
|
|
|
|
|
Release date: 07 Jul 2007
Info modified on: 21 Aug 2008 21:21:39
Legitieme Windows Vista™ Home Premium, Intel® Core™2 Duo processor T7100 1.8GHz (800MHz/2MB), Works 8.5 + Office Home & Student 2007 Trial (60 days), 15.4" TFT WXGA CrystalBrite, 2048MB DDR II RAM (2x 1024), 160GB HDD (5400rpm), Super Multi DVD-RW Double Layer, 6-cell LiIon, 56K modem, Gigabit & Wireless Lan 802.11a/b/g, Up to 1024MB ATI Mobility™ Radeon® HD 2300 HyperMemory(256MB dedicated), 5-in-1 card reader, 0.3MP CrystalEye
|
|
|
|
|
|
A notebook, also known as laptop, is a portable computer. When you are looking for the right notebook, it is important to know where you are going to work with it. Do you want to use it on the road? Choose a model with a special energy saving 'mobile' processor, a good battery and a reasonably small display. This will allow you to work longer with the same battery and saves you the trouble of carrying around a large display that consumes a lot of precious battery power. Or will you be using you notebook mainly in places where you will have access to a power outlet? Then choose a desktop processor (more processing power for less money) and an ordinary battery, this will save you a lot of money, which you could spend on a bigger screen, you'll work faster because you can view more information at once and it's great for multimedia!
|
 |
 |
 |
|
|
The new Aspire 5720 is a clear example of Acer's new Gemstone design philosophy and is the choice for consumers that are looking for state-of-the-art technology and multimedia features. Available with either shared graphics or the latest powerful ATI graphic cards with up to 256MB of dedicated memory the Aspire 5720 offers fantastic value for money. Complete with a 15.4” Acer CrystalBrite display,
...
More>>>
integrated Acer CrystalEye camera and Dolby Digital Live audio it will be the perfect companion for your everyday entertainment needs.
Innovative Design The new Aspire 5720 breaks away from tradition and looks beyond mere benefits and technological advances. The new innovative Gemstone design reflects the changing face of Acer's design awareness without compromizing anything on performance. Latest technology Built on the highly succesful Intel Core 2 Duo CPU generation the new Aspire 5720 offers the latest technology on the market today, with it's large hard disk, integrated Acer CrystalEye webcam, 5-in-1 card reader and the optional HD-DVD drive the Aspire 5720 is meeting the needs of even the most demanding multimedia users.
<<<Less
|
|
 |
Specs
|
Alternatives
|
Options
|
|
|
|
Processor clock speed
|
|
Processor speed in Mhz. Often the clock speed is expressed by a manufacturer in GHz (1 GHz = 1000 MHz). The clock rate is the fundamental rate in cycles per second (measured in hertz) at which a computer performs its most basic operations such as adding two numbers. There are more factors, like internal memory size, that influence a computer's actual response time.
1800 MHz
|
|
Processor family
|
|
The processor serie to which the processor belongs.
Intel Core 2 Duo
|
|
Processor
|
|
Processor is the central unit in a computer containing the logic circuitry that performs the instructions of a computer's programs.
Intel Core 2 Duo T7100
|
|
Processor front side bus
|
|
Speed of the processor's Front Side Bus (FSB) in megahertz (1 million Herz). The FSB is the bus that transfers data between the CPU and the northbridge of the Motherboard. The maximum theoretical bandwidth of the FSB is determined by the product of its width, its clock frequency and the number of data transfers it performs per clock tick.
800 MHz
|
|
Chipset
|
|
Chipset for this configuration; expressed as manufacturer and coined name
Mobile Intel PM965 Express
|
|
L2 cache
|
|
The CPU cache (Level 2 in megabyte) is a smaller, faster memory which stores copies of the data from the most frequently used main memory locations.
2 MB
|
|
Hard disk drive capacity
|
|
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).
160 GB
|
| Hard disk interface |
SATA |
|
Hard disk rotational speed
|
|
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
5400 RPM
|
|
Display diagonal
|
|
Size of the display for this product; expressed in inches diagonal
15.4 "
|
|
Display
|
|
The display technology. Flat screen technologies like Liquid Cristal Display (LCD) and Thin Film Transistor (TFT) active matrix technology are the trend.
In TV technologies one can notice FST (Flat Screen Tube) technology, and ARASC (Anti Reflexion, Anti Static Coating) or AGARAS (Anti-Glare ARASC) or simply AGC (anti-glare coating). The old tv and screen technology CRT means Cathodic Ray Tube. MLA = Micro Lens Array. p-Si=Polycrystalline Silicon. a-Si=Amorphous Silicon.
WXGA TFT LCD
|
| Display response rise/fall |
8 ms |
|
Display resolution
|
|
Resolution of the display for the system
1280 x 800 pixels
|
|
Number of colours
|
|
Maximum number of viewable colors.
16.7 M
|
|
Internal memory
|
|
The amount of memory measured in megabytes installed in the system's hardware
2048 MB
|
|
Memory slots
|
|
Number and type of memory expansion slots; including connector and memory module descriptions
so-DIMM
|
| Internal memory type |
DDR2 SDRAM |
|
Memory layout
|
|
Describe how memory is plugged on the motherboard
2 x 1024 MB
|
| Maximum internal memory |
2 GB |
| Compatible memory cards |
SD/MMC/MS/MS Pro/xD |
| Graphic adapter |
ATI Mobility Radeon HD 2300 HM |
|
Optical drive type
|
|
Type of the optical drive
Super Multi DVD-RW DL
|
| Built-in microphone |
 |
| Audio system |
High Definition Audio |
| Number of built-in speakers |
2 |
| Keyboard function keys |
12 |
| Keyboard number of keys |
88 / 89 |
| Camera included |
 |
|
Megapixel
|
|
MegaPixels: The number (in millions) of light-sensitive picture elements, or pixels, actually used by the camera's image sensor (CCD) to record light, and which are reflected to the final number of recorded pixels stored on the memory card.
0.3 MP
|
| Internal modem |
 |
| Networking features |
Gigabit Ethernet |
| Wake-on-Ring ready |
 |
| Wireless technology |
IEEE 802.11a/b/g |
| Modem speed |
56 Kbit/s |
| Modem type |
ITU V.92 |
| Wake-on-LAN ready |
 |
|
Bluetooth
|
|
Bluetooth is a low-power radio technology developed to replace the cables and wires currently used to link or connect electronic devices such as personal computers, printers, and a wide variety of handheld devices including mobile phones. Because it uses radio-wave connectivity, a Bluetooth-enabled device has a constant, established connection to whatever browser it uses. This saves the user the trouble of logging on to check for emails or news updates, for example.
|
| Wireless LAN data transfer rate (max) |
54 Mbit/s |
| Operating system provided |
Windows Vista Home Premium Edition |
|
| Bundled software |
Acer Empowering Technology (Acer eNet, ePower, eAudio, ePresentation, eDataSecurity, eLock, eRecovery, eSettings Management), Acer GridVista™, Acer Launch manager, Acer Arcade / Arcade™ Deluxe + DV Wizard, VideoMagician, DVDivine, Acer GameZone, Adobe Reader™, CyberLink® PowerProducer®, NTI® CD Maker™ |
| Battery technology |
Lithium-Ion |
|
Battery life
|
|
Maximum battery life in hours. Mobile Mark™ (2002) is the standard often used to benchmark battery life time. In some cases battery life can be extended by adding extra batteries.
2.5 h
|
| Number of battery cells |
6 pcs |
| ExpressCard slot |
 |
| VGA (D-Sub) ports quantity |
1 |
| Ethernet LAN (RJ-45) ports quantity |
1 |
| IEEE 1394/Firewire ports quantity |
1 |
|
TV out port
|
|
Description of TV Out port
S-Video
|
|
USB 2.0 ports quantity
|
|
USB 2.0 ports have a data transmission speed of 480 Mbps, and are backwards compatible with USB 1.1 ports. You can connect all kinds of peripheral devices to them.
4
|
| Modem (RJ-11) ports |
1 |
| Speaker/ headphone/ line-out jack |
 |
| Microphone, line-in jack |
 |
| S/PDIF out port |
 |
| DC-in jack |
 |
| DVI port |
 |
|
Infrared data port
|
|
A data port that uses infra-red data association (irDA) as the standard for wireless communications between computer and mobile phone devices. For example, to update the phone list on your irDA-enabled PC, you would line up the infra-red ports on each device and then transfer the phone information to your PC. This is a wireless transfer, so you don't need a cable or extra software.
|
| SmartCard slot |
 |
| CardBus PCMCIA slot type |
 |
| TV in port |
 |
| Port replicator |
 |
| Cable lock slot |
Kensington |
| BIOS password |
 |
|
Weight
|
|
Weight of the product without packaging (nett weight). If possible, the nett weight is given including standard accessories and supplies. Please, note that sometimes the manufacturer is giving a too commercial interpretation of product weight, by leaving out the weight of accessories and/or supplies.
2900 g
|
|
Dimensions W x D x H
|
|
Dimensions of the produkt (Width x Depth x Height) in millimeter.
366 x 274 x 43 mm
|
| Depth |
274 mm |
|
Height
|
|
Height of the product
43 mm
|
| Width |
366 mm |
| Pointing device |
Touchpad |
|
|
|
|
|
| hard disk drives |
 |
 |
SPE3030CC/00 |
External Hard Disk, 320GB |
|
| keyboards & desktops |
 |
 |
KP002 |
Portable USB Keypad and 2 Port HUB |
|
| network cards & adapters |
 |
 |
DWA-140 |
Wireless N USB Adapter |
|
 |
 |
20002325 |
FRITZ!WLAN USB Stick |
|
 |
 |
3CRUSB10075 |
OfficeConnect Wireless 54Mbps 11g Compact USB Adapter |
|
 |
 |
20002420 |
FRITZ!WLAN USB Stick N |
|
 |
 |
CN-WF518D |
Network Adapter, Wireless, 54Mbps, Retail, IEEE 802.11b/IEEE 802.11g, USB 2.0 |
|
 |
 |
DWA-645 |
RangeBooster N650 Draft-11n PC Card |
|
| Show all network cards & adapters >> | | mice |
 |
 |
CLLMTRAVEL |
Lounge’n’LOOK Travel Mouse |
|
 |
 |
MI015 |
Mini Wireless Optical Mouse |
|
 |
 |
MICROII-EU |
USB optical micro mouse |
|
 |
 |
931669-0914 |
V450 Laser Cordless Mouse for Notebooks |
|
| Show all mice >> | | notebook bags & cases |
 |
 |
NCV1 |
Basic Laptop Case 15.4" |
|
 |
 |
PNC15 |
15.4" Slimline Laptop Case |
|
 |
 |
KLC15 |
15.4" Lightweight Professional Laptop Case |
|
| routers |
 |
 |
3CRWER200-75-ME |
OfficeConnect Wireless 108 Mbps 11g Cable/DSL Router |
|
 |
 |
3CRWER100-75-ME |
OfficeConnect Wireless 54 Mbps 11g Cable/DSL Router |
|
 |
 |
C54BRS4 |
Wireless Router & Access Point |
|
| antivirus & security software |
 |
 |
2869 |
AntiVirus 2008 NL |
|
 |
 |
2870 |
InternetSecurity 2008 NL |
|
 |
 |
2867 |
TotalCare 2008 NL |
|
 |
 |
Q12P08 |
Internet Security 2008, 3-user, 1 Year, NL |
|
 |
 |
Q12T08 |
Antivirus + Firewall 2008, 3-user, 1 Year, NL |
|
 |
 |
KL1125NLBOX |
Kaspersky® Anti-Virus 7.0, CROM, Box, NL |
|
 |
 |
Q12L08 |
Antivirus 2008, 3-user, 1 Year, NL |
|
 |
 |
11057341 |
Norton 360 (NL) WinXP/Vista |
|
 |
 |
KL1825NLBOX |
Kaspersky® Internet Security 7.0, CDROM, Box, NL |
|
 |
 |
ETRAV8001BPEM |
eTrust Avirus r8 NON CD W32 1user |
|
 |
 |
ETRPPCE8001BPEM |
eTrust PestPatrol Corporate Edition r 8in English French Italian German Spanish and Japanese - 1 User - Product only |
|
 |
 |
ETRITM8001BPEM | | | | |